Issue:
Configuring the ATV212 to ignore a communication fault and continue running at the current speed reference
Product Line:
ALTIVAR 212
Resolution:
Set parameter F851 = 1
In case of a network communication loss, the VFD will not go to a fault status, but rather continue with the last commanded operation. If stopped, it will remain stopped. If running, it will remain running at the last speed reference given.
Consider safety ramifications for this action.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for:Schneider Electric Global