Issue:
Trying to set up the ATV61/71 drive so that the set point for PID can be adjusted using the keypad.
Product Line:
ALTIVAR 61, ALTIVAR 71
Environment:
All serial numbers
Resolution:
In the PID Regulator function, set parameter "Act. Internal PID ref" to NO. Use "Ref 1 channel" set to HMI.
Trying to set up the ATV61/71 drive so that the set point for PID can be adjusted using the keypad.
Product Line:
ALTIVAR 61, ALTIVAR 71
Environment:
All serial numbers
Resolution:
In the PID Regulator function, set parameter "Act. Internal PID ref" to NO. Use "Ref 1 channel" set to HMI.
Released for:Schneider Electric Global