Issue:
Mounting an ATV212 drive in a Nema 3R enclosure.
Product Line:
ATV212
Environment:
All serial numbers for ATV212
Cause:
N/A
Resolution:
Yes. The drive comes as an IP20 open style unit and can be mounted in any customized enclosure.
Please reference the attached installation manual for dimensions, weight, mounting tips, air flow, heat dissipation and more
Mounting an ATV212 drive in a Nema 3R enclosure.
Product Line:
ATV212
Environment:
All serial numbers for ATV212
Cause:
N/A
Resolution:
Yes. The drive comes as an IP20 open style unit and can be mounted in any customized enclosure.
Please reference the attached installation manual for dimensions, weight, mounting tips, air flow, heat dissipation and more
Released for:Schneider Electric Global