{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is there a variable for the elapse time in a Timer block in EcoStruxure Machine Expert-Basic / SoMachine Basic?
Issue:
Is there a variable for the elapse time in a Timer (%TM)  block in EcoStruxure Machine Expert-Basic / SoMachine Basic?

Product Line:
EcoStruxure Machine Expert-Basic / SoMachine Basic
Modicon M221 PLC

Environment:
PLC Programming Software Windows

Resolution:
In EcoStruxure Machine Expert-Basic / SoMachine Basic programming software, the Elapsed Time for a Timer (%TM) block is stored in %TMx.V, where x is the timer instance number starting from 0. This value is a Read-only value.
The value will be in the same time format as the Timer block's programmable Time base unit (1ms, 10ms, 100s, 1s, or 1min) .

For a full guide, please refer to the section called Software Objects > "Timer (%TM)" in the EcoStruxure Machine Expert - Basic, Generic Functions Library Guide.
Link to PDF: https://www.se.com/ww/en/download/document/EIO0000003289/

Schneider Electric Global