Issue:
Wiring diagrams for the VW3A3201 and VW3A3202 ATV61/71 option cards.
Product Line:
Altivar ATV61/ATV71
Environment:
All
Cause:
Needs a basic wiring diagram for the VW3A3201 and VW3A3202 option cards.
Resolution:
You can find both of the wiring diagrams in the ATV61 and ATV71 installation manuals.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for:Schneider Electric Global