Issue:
Otr motor torque parameter calculated on the ATV61 and ATV71 drives.
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
N/A
Resolution:
The torque of the motor (OTR) is not measured by the drive. It is calculated from the measurement of motor current.
OTR = (Iq / Iqn) * (PhirdRef / Phirn) in %
With: Iq : Current torque provide by the command to drive motor
PhirdRef : Flux provide by the command to drive motor
Iqn : Nominal Current torque compute with the motor name plate
Phirn : Nominal flux of the motor
The maximum accuracy of motor torque is 5% (in closed loop). It can be up to 15% in open loop.
Concerning the range, OTR is expressed in % of nominal motor torque.
100% = Nominal motor torque.
OTR value is signed with minimum value -300% and maximum value 300%
Otr motor torque parameter calculated on the ATV61 and ATV71 drives.
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
N/A
Resolution:
The torque of the motor (OTR) is not measured by the drive. It is calculated from the measurement of motor current.
OTR = (Iq / Iqn) * (PhirdRef / Phirn) in %
With: Iq : Current torque provide by the command to drive motor
PhirdRef : Flux provide by the command to drive motor
Iqn : Nominal Current torque compute with the motor name plate
Phirn : Nominal flux of the motor
The maximum accuracy of motor torque is 5% (in closed loop). It can be up to 15% in open loop.
Concerning the range, OTR is expressed in % of nominal motor torque.
100% = Nominal motor torque.
OTR value is signed with minimum value -300% and maximum value 300%
Released for:Schneider Electric Global