Issue:
Range of potentiometer used on ATV212 Drives.
Product Line:
ATV212, S-Flex
Environment:
All
Cause:
Need to select a speed pot.
Resolution:
The speed pot range is 2.2 to 10 KOhms. Can use the ATVPOT part number which is 2.5 KOhms speed pot.
Range of potentiometer used on ATV212 Drives.
Product Line:
ATV212, S-Flex
Environment:
All
Cause:
Need to select a speed pot.
Resolution:
The speed pot range is 2.2 to 10 KOhms. Can use the ATVPOT part number which is 2.5 KOhms speed pot.
Released for:Schneider Electric Global