Issue
Cannot change the HTTP or FTP password for the BMXNOE0110 using Web Designer.
Product Line
BMXNOE0110
Environment
Windows 10
Resolution
The selection for HTTP and FTP password on the target security window is greyed out and not selectable.
Due to cyber security reasons, the ability to change the HTTP and FTP passwords for BMXNOE0110 Factorycast
module using Web Designer is not allowed. Changing of the passwords for the BMXNOE0110 Factorycast module
must be performed from the 'Setup' web pages.
Cannot change the HTTP or FTP password for the BMXNOE0110 using Web Designer.
Product Line
BMXNOE0110
Environment
Windows 10
Resolution
The selection for HTTP and FTP password on the target security window is greyed out and not selectable.
Due to cyber security reasons, the ability to change the HTTP and FTP passwords for BMXNOE0110 Factorycast
module using Web Designer is not allowed. Changing of the passwords for the BMXNOE0110 Factorycast module
must be performed from the 'Setup' web pages.
Released for:Schneider Electric Global