Issue
Cannot change the FTP password for the TSXWMY100 using Web Designer.
Product Line
Ethernet Module Premium
Environment
TSXWMY100
Resolution
The selection for FTP password on the target security window is greyed out and not selectable.
Due to cyber security reasons, the ability to change the FTP password for TSXWMY100 Factorycast HMI module using
Web Designer is not allowed. Changing of the FTP password for the TSXWMY100 Factorycast HMI module must be
performed from the 'Setup' web pages.
Released for:Schneider Electric Global