Issue
What is the limitation on the service port of a 140NOC78100?
Product Line
Quantum, 140NOC78000
Resolution
According to the product spec, port 1 (service port) has ingress rate limiting as follows:
What is the limitation on the service port of a 140NOC78100?
Product Line
Quantum, 140NOC78000
Resolution
According to the product spec, port 1 (service port) has ingress rate limiting as follows:
- Unknown unicast, broadcast rate limit = 500 pps
- Arp rate limit = 500 pps
- Multicast rate limit = 30%
- known unicast rate limit = 30%
Released for:Schneider Electric Global