{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the degree of protection rating for the ATVPOT25K?


Resolution:
This kit includes the ZB5AD922 operator which is rated for Nema 1, 2, 3, 4, 4X, 12, 13.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:Frequently Asked Questions - Schneider Electric (se.com)If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.If you are not located in North America, please contact your local Customer Care Center for assistance:Support | Schneider Electric Global (se.com)