Issue:
Setup for analog output or AO1 on ATV61 & ATV71.
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
Needs to set up the analog output for frequency with min 4mA and max 20mA.
Resolution:
Programming
Menu 1.5 I/O or inputs and outputs
AO1 assignment
Assign to motor frequency
Type: current
Min 4mA Max 20mA
Setup for analog output or AO1 on ATV61 & ATV71.
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
Needs to set up the analog output for frequency with min 4mA and max 20mA.
Resolution:
Programming
Menu 1.5 I/O or inputs and outputs
AO1 assignment
Assign to motor frequency
Type: current
Min 4mA Max 20mA
Released for:Schneider Electric Global