Yes it is possible to use the mechanical interlock by cables for MTZ/NW/NT breakers inside the BlokSeT column.
Below is the procedure which needs to be followed to have this solution inside the BlokSeT.
2. Masterpact catalog gives source changeover to assemble in different combinations.
Below is the procedure which needs to be followed to have this solution inside the BlokSeT.
- The U-channel of the column should be cut as shown. The dimension of material to be removed is 200 x 25 as shown below.
2. Masterpact catalog gives source changeover to assemble in different combinations.
Released for:Schneider Electric Global