{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How is works the SIM10M digital input ?
SIM10M digital input is not normal digital inputs where you apply a certain voltage. These digital inputs does only detect a closed circuit (to ground, "sinking currentt")
When an input is connected to ground, a small current is generated (1mA  limited by internal 2.2kOhm resistor)  and measured by the SIM, and a pulse is recorded. The pull-up resistor is 2.47 kohm.
The minimum pulse length is 5 ms, with maximum  frequency 8Hz.
The maximal cable length between meter and SIM digital input  can be  up to 80 meters but it's recommend 40 meters.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.