Issue
The compatibility of switchboard cases across the ION8xxx meter series.
Product Line
PowerLogic ION8300, ION8400, ION8500, ION8600, ION8650 meters
Environment
Advanced Revenue Metering
Cause
The user would like to use the pre-existing switchboard case when replacing the meter.
The compatibility of switchboard cases across the ION8xxx meter series.
Product Line
PowerLogic ION8300, ION8400, ION8500, ION8600, ION8650 meters
Environment
Advanced Revenue Metering
Cause
The user would like to use the pre-existing switchboard case when replacing the meter.
Resolution
Provided that the replacement meter and the switchboard case are of the same form factor then the two are interchangeable.
Released for:Schneider Electric Global