Background:
Customer is using BMXFCW503 on BMXDDI3202K for a project which requires the flame retardant. The datesheet of BMXFCW503 has no such characteristic announced.
Question:
Is BMXFCW503 flame retardant?
Answer:
Yes, it is flame retardant which is listed in cable SPEC(35013778_E06000)
Customer is using BMXFCW503 on BMXDDI3202K for a project which requires the flame retardant. The datesheet of BMXFCW503 has no such characteristic announced.
Question:
Is BMXFCW503 flame retardant?
Answer:
Yes, it is flame retardant which is listed in cable SPEC(35013778_E06000)
Released for:Schneider Electric Global