{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
New Release of PM3200 driver for PME 8.0 and Register List
Issue
A client has upgraded the PM3200 meter to firmware 1.2.003 and thus not supported in PME 8.0.

Product Line
Power Monitoring Expert 8.0 with PM3200 meter

Environment
Driver update in PME 8.0

Cause

This update resolves the following issues:

- Alarms were not being downloaded after alarm log roll-over.
- Jitter correction for onboard logs (+/- 5 secs)

Resolution
The SE package has the PM3200 driver for PME 8.0 exe file, release notes document and mapping details/register list are attached below.

To install the driver, follow the steps below:

1. Run the 'PM3200_Series_SE_8.0.15355.01_Setup.exe' file.
2. Select the preferred language and click Next to proceed with installation.
3. Follow the on-screen procedure to verify the system, prepare for upgrade by performing backups and configure the system.
4. Once the installation is complete, click Close to exit. The update driver should now should appear under 'Device Types' within Management console.

Schneider Electric Global

Attachment(s)
PM3200_Series_SE_8.0.15355.01_Setup.exe [4.34 MB]
PM3200_Series_SE_8.0.15355.01_Mapping.xlsx [73.98 KB]
PM3200_Series_SE_Driver_Release_Notes_PME 8.0.pdf [3.06 MB]