Issue:
Asking about parameter F400 on the ATV212.
Product Line:
Altivar 212, Altivar 21
Environment:
All Serial numbers
Cause:
N/A
Resolution:
F400 is the auto tuning parameter for the ATV212 and the ATV21. The setting for the parameters are listed below:
0 [Deactivated]
1 [Initialize constant] Auto-tuning is performed immediately if possible. Application of individual settings of Auto Torque Boost [Auto
Torque Boost] (F402)
2 [Complete tune] Complete auto tuning.
Parameter F400 is reset to “0” after the auto tuning is performed.
Asking about parameter F400 on the ATV212.
Product Line:
Altivar 212, Altivar 21
Environment:
All Serial numbers
Cause:
N/A
Resolution:
F400 is the auto tuning parameter for the ATV212 and the ATV21. The setting for the parameters are listed below:
0 [Deactivated]
1 [Initialize constant] Auto-tuning is performed immediately if possible. Application of individual settings of Auto Torque Boost [Auto
Torque Boost] (F402)
2 [Complete tune] Complete auto tuning.
Parameter F400 is reset to “0” after the auto tuning is performed.
Released for:Schneider Electric Global