{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do you program the ATV312 drive to be controlled by the optional VW3A31101 remote keypad display?
Issue:
Programming the ATV312 drive to be controlled by the VW3A31101 remote keypad display.

Product Line:
Altivar

Environment:
All

Cause:
Wants to use the VW3A31101 remote keypad display for speed and start  stop control

Resolution:
Programming
RDY menu enter scroll down to CTL menu enter
CTL menu scroll down LAC make sure you are in L1 or level 1
CTL menu scroll down to LCC enter and set this to Yes.
LCC= Keypad control

Schneider Electric Global