{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: How do you set a run permissive on an ATV312 drive?

Article available in these languages: Spanish

Issue:
ATV312 how to set up a permissive run

Product Line:
Altivar 312, ATV312

Environment:
All

Cause:
Safety, permissive function.

Resolution:
In the programming, go into menus FUn-, StC-, and parameter nSt.  Assign nSt to a logic input LIx to act as a permissive.
If that corresponding logic input does not have a +24VDC applied, the drive will show nSt on the display to indicate freewheel stop status.
The freewheel stop / run permissive function applies for both Local and Remote modes of operation.