{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the error code MOFF on the ATV212?

Article available in these languages: Spanish

Issue:
Meaning of error code MOFF on the ATV212.

Product Line:
Altivar 21, Altivar 212

Environment:
All serial numbers

Cause:
Drive faulting on under voltage

Resolution:
Code MOFF indicates that the phase-to-phase input voltage is too low.   Measure the main circuit supply voltage.  If the voltage is normal for the VFD, check the connection of the factory jumper on PO and PA+ terminals.  MOFF is an alarm condition and does not put the VFD into a faulted state.