Issue
After adding a Rockwell CPUs (such as Compactlogix ones) EDS files in the DTM catalog, we can’t “add connections" in order to exchange data between the NOC or SE CPU and those Rockwell CPU.
Product Line
BMENOC, M580
Resolution
This is an EDS file of a Rockwell CPU (Micrologix in this case) in Note pad:
$ EDS file for 1766-L32
$
$ Revision history:
$
$ 1.1 09-17-2007 Initial Version for ML1400 Series A.
$ 2.1 09-07-2009 Supports ML1400 Series B.
$
[File]
DescText = "MicroLogix1400 EDS";
CreateDate = 09-17-2007;
CreateTime = 16:14:00;
ModDate = 09-07-2009;
ModTime = 13:50:00;
Revision = 2.1;
HomeURL = "http://www.ab.com/networks/eds/EN/0001000E005A0200.eds";
[Device]
VendCode = 1;
VendName = "Rockwell Automation Allen-Bradley";
ProdType = 14;
ProdTypeStr = "Programmable Logic Controller";
ProdCode = 90;
MajRev = 2;
MinRev = 8;
ProdName = "MicroLogix1400";
Catalog = "1766-L32";
Icon = "MicroLogix.ico";
1_Revision_Alpha = Yes;
[Port]
Port2 = TCP, "Channel 2", "20 F5 24 01", 2;
[Device Classification]
Class1 = EtherNetIP;
This clearly shows no communication parameters and connections available. We can notice the difference with the EDS file for a connexium switch for example.
Therefore, there is no way to add a connection to that EDS file; this means that this Micrologix controller doesn't support implicit messaging.
We then recommend to use explicit messaging via the DATA_EXCH block
Released for:Schneider Electric Global