Issue:
Is there an option for the Altivar drives to connect using a RS232 connection?
Product Line:
Alitivar
Environment:
All
Cause:
Product Selection & Services
Resolution
No, converter options for RS232 to RJ45. There is a cable available for a RJ45 to USB part number TCSMCNAM3M002P USB to RJ45
adaptor
For use in connecting to a PC with a USB port
Advantys™ OTB,
Altistart™ motor starters,
Altivar series including
HMI, Altivar controller
Is there an option for the Altivar drives to connect using a RS232 connection?
Product Line:
Alitivar
Environment:
All
Cause:
Product Selection & Services
Resolution
No, converter options for RS232 to RJ45. There is a cable available for a RJ45 to USB part number TCSMCNAM3M002P USB to RJ45
adaptor
For use in connecting to a PC with a USB port
Advantys™ OTB,
Altistart™ motor starters,
Altivar series including
HMI, Altivar controller
Released for:Schneider Electric Global