PowerChute Network Shutdown remaining runtime threshold does not trigger OS shutdown when communicating with SURTD when NMC 1 is installed.
Published date:
29 January 2019
Issue:
PowerChute Network Shutdown remaining runtime threshold does not trigger OS shutdown when communicating with SURTD when NMC 1 (AP9617, AP9618, AP9619) is installed. The OS remains running until the UPS reaches low battery and then the OS is commanded to power down due to low battery.
Product Line:
PowerChute Network Shutdown
Environment:
All supported OS
Cause:
SURTD reports the remaining runtime to PowerChute in seconds when PowerChute is expecting to receive the time in minutes.
Solution:
PowerChute expects the threshold to be entered in seconds so to compensate for the difference in time multiply time by 60.
Shutdown Examples
Shut OS down when UPS fails below 25 minutes = 1500 seconds x 60 = 90000 seconds
Shut OS down when UPS fails below 20 minutes = 1200 seconds x 60 = 72000 seconds
Shut OS down when UPS fails below 15 minutes = 900 seconds x 60 = 54000 seconds
Shut OS down when UPS fails below 10 minutes = 600 seconds x 60 = 36000 seconds
Another option is to replace the NMC with AP9630 or AP9631. The AP9630 and AP9631 do not exhibit the issue.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.