{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is the S-Flex drive available in Nema 3R outdoor enclosure?
Issue:
Is the S-Flex drive available in Nema 3R outdoor enclosure?

Product Line:
S-Flex

Environment:
3R enclosure

Cause:
n/a

Resolution:
Yes, They are available in Nema 1, Nema 12, and Nema 3R.
Nema 12 and 3R units have a longer lead time because they are not stocked and must be built to order through product selector.