{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Smart-UPS VT-G3500; Load does not turn on automatically after an outage/shutdown

Article available in these languages: Spanish


Issue:
Load does not turn on automatically after an outage/shutdown


Product line:
Smart-UPS VT-Galaxy 3500


Environment:
All Product models, all serial numbers


Cause:
The system is set to not auto start by default


Resolution:
You can set the load to turn on automatically after an outage from the PowerView display.

1. Go to Setup menu
2: Select System
3: Select Auto Start
4. Change value to On

This may take one reboot of the UPS to take affect, and you will need to turn on the load manually then.  After that first reboot it should automatically turn on in the future.