{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Used Plastic Material Details in PM3200

1- Weights of plastic or other flammable materials (printed circuit boards)

Approximately 240 grams per meter


2- Plastic details (Yellow Card- number according to UL 94) / the UL94 Flammability classification

Enclosure material :  Lexan  505RU or Lexan 945, rated V0.
Panel cover(Lens) material : Lexan  923A , rated V2.
Attached UL yellow card for the plastics.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.