{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does the ATS48 have a built in Shorting Contactor?
Issue:
Is the ATS48 built with shorting contactor?

Product Line:
ATS48

Environment:
Shorting contactor

Cause:
n/a

Resolution:
No, the ATS48 does not have a built-in Shorting contactor.  But the ATS22 is the only soft start with a built-in Shorting contactor.