{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Where can I find the Profibus GDS files for ATV61 and ATV71?
Issue:
Needs the GDS files for Profibus

Product line:
ATV61, ATV71

Environment:
all

Cause:
n/a

Resolution:

See the attached file package.

There were 2 versions of the Profibus option card.  The first to be released was VW3A3307 and supported DP0.
An updated version (VW3A3307S371) was later released that supported both DP0 and DP1.
GSD files for both versions cards are attached.

Schneider Electric Global

Attachment(s)
ATV61_71_Profibus_DPv0_files.zip [3.55 KB]
ATV61-71_ProfibusDP_v1.zip [9.44 KB]