Issue:
Braking capacity ATV312HU15N4
Product Line:
ATV312
Environment:
All
Cause:
Braking capacity ATV312
Resolution:
Without a braking resistor, it is 50% of nominal motor torque. With braking resistor, it is 100% of motor torque continuous and 150% of torque for 60 seconds.
Braking capacity ATV312HU15N4
Product Line:
ATV312
Environment:
All
Cause:
Braking capacity ATV312
Resolution:
Without a braking resistor, it is 50% of nominal motor torque. With braking resistor, it is 100% of motor torque continuous and 150% of torque for 60 seconds.
Released for:Schneider Electric Global