{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Do I need the VW3A1105, RJ45 female to female adapter if I order a remote mount kit VW3A1102?
Issue:
Remote mounting kit VW3A1102 specifications

Product Line:
ATV61, ATV71, ATV212, ATV32, ATV312

Environment:
Any drive that uses the VW3A1101 keypad

Cause:
None

Resolution:
VW3A1105 RJ-45 female—female adaptor is used to connect the LCD Graphic keypad and cable. It is not required if using VW3A1102.

Schneider Electric Global