The default setting for Type of Stop on the ATV312 drives is Ramp stop.
The options for stopping are:
- Ramp
- Freewheel
- Fast Stop
- DC Injection.
Programming below is showing the drive code and in brackets, (text using the VW3A1101 remote HMI display)
To access the Stop Mode, go to the FUn- (Application function) menu, then StC- (Stop Mode) then Stt (Type of stop). The options are:
- rNP (Ramp)
- FSt (Fast stop)
- nSt (Freewheel)
- dCI (DC Injection)
Please note that nSt (Freewheel), FSt (Fast stop) and dCI (DC Injection) can also be assigned to other logic inputs under the StC- (Stop Modes) menu.
Released for:Schneider Electric Global