{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does a harsh environment BMXNRP0200 exist?
Issue
Does a harsh environment BMXNRP0200 exist?

Product Line
M580

Resolution

A hardened version of the BMXNRP0200 module is not possible without a redesign, however we are able to conformal coat them.

Here are the different part numbers:

BMXNRP0200 = suitable for use in standard operating environments

BMXNRP0200C = suitable for use in standard temperature environments with pollution (gas, humidity, dust)

BMXNRP0200T = suitable for use in extreme temperature environments (-25...70 °C) with no pollution

Schneider Electric Global