Issue
How long is the application or data stay in the Flash memory of a M580?
Product Line
M580
Resolution
Once data or application are stored on flash memory, no energy is needed anymore (same than your data on USB key, since all USB keys are made of Flash memory) => we consider 10 years, but this is an average value for Flash technology and it is more than enough for our controllers!
Released for:Schneider Electric Global