{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to delete a DTM in a Unity pro application when not installed - M580 platform
Issue

Error message displayed when trying to delete a DTM
Potential issue due to the DTM version Compatibility"
"Warning: Potential issue due to the DTM version incompatibility.  xxx DTM.
An error occurs during the check of DTM compatibility. DTM version in application is Vxxx).
DTM on the PC: not installed or installed without version information

Product Line

M580, BMENOC0301, BMENOC0311

Resolution

As of today, when a DTM is not installed,  it is impossible to create the dynamic menu of the Dtm and then delete it.

We suggest to
  • Install the required DTM
  • Update the DTM catalog
  • Open the application and the TOOL>DTM browser
  • Delete the desired DTM from the DTM browser tree.

Schneider Electric Global