Video: How to set an ATV61/71 drive for feedback (analog output) to show motor frequency?
Published date:
26 April 2019
Issue:
How to set an ATV61/71 drive for feedback to show motor frequency?
Product Line:
Altivar 61, Altivar 71
Environment:
All models
Cause:
Feedback delivery from drive
Resolution:
Go to Menu 1 [Drive Menu] and then to 1.5 [Inputs/Outputs CFG].
Go to AO1 Configuration.
Set AO1 Assignment to motor freq.
Set analog output type to desired value (Voltage or Current).
Set AO1 min Output and AO1 max Output as needed. Typical options include 0-10VDC, 0-20mA, or 4-20mA.
Go to Menu 1.1 [Simply Start] or Menu 1.4 [Motor Control]
Set Max Frequency and set to 60 Hz to scale the analog output between 0 and 60 Hz.
Set Max Frequency to 50 Hz to scale the analog output between 0 and 50 Hz.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.