{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the impedance of the analog input AI1 on the ATV12 drive?

Article available in these languages: Spanish

Issue:
Impedance of the ATV12 Analog input AI1.

Product Line:
All ATV12 drives

Environment:
Analog input 1

Cause:
None

Resolution:
Analog input AI1 can be configured as a voltage input or current [AIIt = 5U, 10U or 0A].
Analog voltage input can be configured 0 to +5 V or 0 to +10 V (maximum voltage 30 V).  the impedance: 30 kΩ.
Analog current input x to y mA, has an impedance of 250 Ω.

Schneider Electric Global