Issue
Does the Modicon M241 HSC support periodic meter measurement?
Product Line
Modicon M241 PLC
Environment
HSC (High Speed Counter) feature in PLC
Resolution
Yes, the Modicon M241 controller supports up to 2 channels using the Fast input that can be setup as period meter.
Periodic measurement calculates the period between two events.
Does the Modicon M241 HSC support periodic meter measurement?
Product Line
Modicon M241 PLC
Environment
HSC (High Speed Counter) feature in PLC
Resolution
Yes, the Modicon M241 controller supports up to 2 channels using the Fast input that can be setup as period meter.
Periodic measurement calculates the period between two events.
Released for:Schneider Electric Global