Issue:
Needs to know the baud rate for ATS48 modbus
Product Line:
ATS48
Environment:
All
Cause:
Need to use 115.2 baud
Resolution:
ATS48 modbus is only available at 19200 or 9600.
Please note that the remote HMI only works with the 19200 baud rate.
Needs to know the baud rate for ATS48 modbus
Product Line:
ATS48
Environment:
All
Cause:
Need to use 115.2 baud
Resolution:
ATS48 modbus is only available at 19200 or 9600.
Please note that the remote HMI only works with the 19200 baud rate.
Released for:Schneider Electric Global