{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do I bring a Standby CPU online which has mismatched firmware in a Control Expert (formerly Unity Pro) Quantum HSBY application ?
Issue:N/A
Product Line: Quantum
Environment: N/A
Cause: N/A


You can bring the Standby online by logging into the Primary CPU and setting %SW60 to a value of 22 decimal. After setting %SW60 to 22, power cycle the Standby .
Once the Standby is online, you can return set the value of %SW60 to 6 decimal.

Use this tip as a temporary solution . You do not want to run HSBY for an extended period of time with this bit mask. The purpose of this feature is to allow the user
to update CPU firmware in an HSBY application without having to shut down.

R-6-30-17