Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

		
Search FAQs
PME OPC Test Client: Could not load file or assembly 'OpcRcw.xx'

Issue
Within the PME OPC Test Client, when attempting to connect to an OPC client, the software returns the following error: Could not load file or assembly 'OpcRcw.Ae'.. or one of its dependencies. The system cannot find the specified file.

Pop-up window with error message "Could not load file or assembly" for OPC Test Client issue

Product Line
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024



Environment
PME OPC Test Client

Cause
This error is caused by the 'OpcRcw.xx' files becoming corrupted.

Or

Power Monitoring Expert is unable to load the file or the defined assembly.

Resolution
**Warning: Take backups of any files before modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).

Use the Power Monitoring Expert installation media to replace the OpcRcw.xx dll files within the "Power Monitoring Expert\system\bin" folder

  1. Obtain the Power monitoring Expert installation media that you are working with
    1. PMe installation media example
  2. Right-click the installation media and select "Mount"
    1. mount example
  3. Use the File Explorer to navigate to the computer's DVD Drive where the Power Monitoring Expert installation media will be mounted
  4. Once here, navigate to the following file path in the PME installation media -> DVD Drive ():\Setup\SetupSupport\OPC\setup.exe
    1. file explorer example
  5. Right-click the "setup.exe" and select "Run as Administrator"

The OPC test client software should re-connect to the OPC client server without restarting the 'ION OPC Data Access Server' service.

If you encounter this error at installation:

.NET Framework error


Verify the version of .NET Framework in the registry.

  1. In the Windows Search bar type "Run" and select the program.
  2. In Run, search for "regedit"regedit and select OK.
  3. Navigate to HKLM\Software\Microsoft\NET Framework Setup\NDP\v3.5. Confirm that .NET Framework 3.5 is installed. .NET Framework includes the feature set from .NET 2.0 and 3.0.

.NET Framework 3.5

If .NET Framework 3.5 is not installed, navigate to "Turn Windows Features on or off" and turn .NET Framework 3.5 on.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Our Mission
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Financial Results
  • Annual Reports
  • Share Price
  • Investor Events
  • Careers
  • Sustainability
  • Electricity 4.0
  • Next-generation Automation
  • AI and Technology
  • Reports
  • Foundation
  • Consulting
  • Global - FR
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Change your cookie settings