{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What to do when Vijeo Designer cannot delete objects from the Favorites folder in the toolchest?
Issue:
What to do when Vijeo Designer cannot delete objects from the Favorites folder in the toolchest?

Product Line:
Vijeo Designer 6.2

Resolution:
When you are unable to delete objects from the Favorites folder of the Toolchest, goto the following folder and set the read/write permissions on the file TCParts.tcp.

"C:\Users\Public\Documents\Vijeo-Designer 6.2\ToolChest"

Restart Vijeo Designer and try again.