Issue:
ATV32 parameter that will allow to reverse the output phase rotation
Product Line:
Altivar 32 series
Environment:
All models, All serial numbers
Cause:
Can not find a parameter to do this in current literature.
Resolution:
The ATV32 series drive does not have a means to reverse the output phase rotation via programming parameter. To reverse the direction of the motor, swap 2 leads on the output side of the drive. If you swap phase rotation on the input side of the ATV32, the motor direction will not change.
ATV32 parameter that will allow to reverse the output phase rotation
Product Line:
Altivar 32 series
Environment:
All models, All serial numbers
Cause:
Can not find a parameter to do this in current literature.
Resolution:
The ATV32 series drive does not have a means to reverse the output phase rotation via programming parameter. To reverse the direction of the motor, swap 2 leads on the output side of the drive. If you swap phase rotation on the input side of the ATV32, the motor direction will not change.
Released for:Schneider Electric Global