Issue
User observes a number of error messages from the meter related to V NegSeqMag with Voltage Unbalance Count N1 limit exceeded
Product
ION 7650
ION 8650
Environment
Power Monitoring Expert (PME)
StruxureWare Power Monitoring (SPM)
ION Setup
Cause
The events are coming from the Signal Limit Evaluation Module. Every 10 minutes the module will evaluate the Source and Nominal inputs and increment the Valid or Invalid outputs. Only the Invalid outputs are incrementing which is triggering the events. The root cause is the Phase rotation setting in the meter does not match the physical system.
Resolution
Change the phase order setup register
In ION Setup
1) Connect to the meter
2) Place the meter in Advanced configuration mode (refer to ION Setup help for more information if required)
3) Select the power meter modules folder
4) Double click on the Power Meter Module
5) Under setup registers, change the setup register PhaseOrder to match the system. Options are either ABC or ACB.
6) Send changes to the meter
7) Close ION Setup
In Designer
1) Open the meter node in Designer
2) Navigate to the Power Meter Module
3) Right click on the module to enter setup window
4) Under the setup registers modify the PhaseOrder register to match the system
5) Close the meter node inside designer then close designer
Released for: Schneider Electric Global