{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why can't I upload my IEC program from my Concept PLC?
Issue:
IEC code in the PLC not available for upload.

IEC
Product Line:
Concept programming software.

Cause:
Either the project was downloaded before Concept 2.5 SR2 which is when IEC upload was added or
The IEC upload switch was not engaged when the project was originally downloaded.

Resolution:
There is no workaround for this problem.
The customer can avoid it in the future by opening the project offline and going to <Project><Code generation options...> and
checking <Include IEC upload information>.  This should be followed by a full download to the PLC.

Schneider Electric Global