{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can a Quantum IO module be hot swapped?
Yes. However this must be done by a qualified individual who is familiar with the inputs or loads associated with the module.
You need to be aware of how the loss of signal input or control output can effect the application.\ before performing the swap.

Quantum CPU's should never be hot swapped.
Don't hot swap a stand alone power supply in the main PLC rack as it will result in a corrupted project.



R-72417

Schneider Electric Global