Issue:
What faults can be reset with the automatic restart on ATV61/71?
Product Line:
Variable Frequency Drives
Environment:
Applies to Altivar 61/71
Cause:
Customer wants to know if he can automatically restart the drive after a fault
Resolution:
Faults that can be reset with automatic restart function, after the cause has disappeared:
APF, CnF, COF, EPF1, EPF2, FCF2, Fd1, LFF2, LFF3, LFF4, nFF, ObF, OHF, OLC, OLF, OPF1, OPF2, OSF, OtF1, OtF2, OtFL, PHF, PtF1, PtF2, PtFL, SLF1, SLF2, SLF3, SPIF, SSF, tJF and ULF
NOTE: In order for the Automatic Restart function to clear a fault and attempt a restart, ALL of the following must be true:
These faults that can be cleared by Automatic Restart are listed in the ATV61 and ATV71 Programming Manuals.
ATV61 Programming Manual:
https://www.se.com/us/en/download/document/1760649/
ATV71 Programming Manual:
https://www.se.com/us/en/download/document/1755855/
What faults can be reset with the automatic restart on ATV61/71?
Product Line:
Variable Frequency Drives
Environment:
Applies to Altivar 61/71
Cause:
Customer wants to know if he can automatically restart the drive after a fault
Resolution:
Faults that can be reset with automatic restart function, after the cause has disappeared:
APF, CnF, COF, EPF1, EPF2, FCF2, Fd1, LFF2, LFF3, LFF4, nFF, ObF, OHF, OLC, OLF, OPF1, OPF2, OSF, OtF1, OtF2, OtFL, PHF, PtF1, PtF2, PtFL, SLF1, SLF2, SLF3, SPIF, SSF, tJF and ULF
NOTE: In order for the Automatic Restart function to clear a fault and attempt a restart, ALL of the following must be true:
- The cause of the original fault must be resolved
- The drive must be set up for 2 wire control
- 2-wire type set to level
- Drive controlled by the drive's terminals
- The run command must be maintained
These faults that can be cleared by Automatic Restart are listed in the ATV61 and ATV71 Programming Manuals.
ATV61 Programming Manual:
https://www.se.com/us/en/download/document/1760649/
ATV71 Programming Manual:
https://www.se.com/us/en/download/document/1755855/
Released for:Schneider Electric Global