{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Unity Pro V11.0 Incomplete Build change, Fail GCC Compilation error
Goals and Symptoms
On BME P58 5040(C) , BME P58 6040(C) and BME H58 6040(C) PLCs application, with Unity Pro V11.0, build change of an application can be incomplete, a section can be not taken in account.
This situation is reported by following WARNING message: Fail GCC Compilation error in the output windows.
But this message does not stop the Build of the application.

Causes and Fixes
install the hotfix UnityPro_V110 HF0337840R to fixes the issue on Unity Pro V11.0.
Unity Pro V11.1 corrects this misbehavior.

Schneider Electric Global