{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is Resi 9 electrical panel and trunking system compatible with competitors products/systems?
YES . The Resi9 electrical panels can be installed on trunking directly with Hager products and Legrand products (Gamma Hager and Legrand Drivia). Conversely Drivia and Gamma units can be installed directly on the Resi 9 trunking .
For other offers, not Schneider control panels, installation on Resi9 trunking system can be made using the universal media.
References: R9H13537 (13Modules) and R9H13541 (18 Modules)

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.