{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Do we offer roof fans for 1200 mm deep cabinets? If not, why not?
Issue:
Is there a roof fan for the 1200 mm deep cabinets?

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
There is a request for a roof fan on a deep cabinet.

Resolution:
We do not currently offer a roof fan for the 1200 mm deep cabinets. If a customer requires a 1200 mm deep roof fan we can process a custom request. Please contact Sales and advise the quantity needed and required ship date.
The roof fans are offered for 1070 mm cabinets primarily because, when loaded with cabling, PDUs, etc, air flow can become a challenge. The fan tray helps to alleviate that issue. Similarly, adding space in the back by moving to a deeper cabinet tends to accomplish the same thing.

Schneider Electric Global